Question, input slow signal into GPIO of i.MX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question, input slow signal into GPIO of i.MX28

1,184 次查看
Aemj
Contributor IV

Hi team,

I would like to ask about the input signal to GPIO of i.MX28.

According to i.MX28 datasheet(Table 25 Digital Pin DC Characteristics for GPIO in 3.3-V Mode), GPIO input ports have 0.8V-2V of threshold voltage.

In my customer’s board, some GPIO pins are used for input signals which have slow rise/fall time. For the input signals from external, it takes about 1mSec to cross the threshold range of 0.8-2V.

My customer worries whether such input to GPIO could affect to the reliability of i.MX28.

Are there any problems for that?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
2 回复数

1,114 次查看
Yongxin
NXP Employee
NXP Employee

Dear Miyamoto-san,

No, there is no problem for the 1ms threshold time form VIL to VIH. From Table 27 of the datasheet, the input buffer is hysteresis function.

Best Regards,

Yongxin

0 项奖励
回复

1,114 次查看
Aemj
Contributor IV

Dear team,

Sorry for harrying you up but my customer is pushing me.

I would appreciate it as early as possible.


Thanks,

Miyamoto

0 项奖励
回复