Hello,
Yes, the mentioned in the Datasheet(s) "four clock inputs to the CCM from normal GPIO pads via IOMUX
can be used as the clock sources in the CCM", are the following:
CCM_EXT_CLK1 on GPIO1_IO00
CCM_EXT_CLK2 on GPIO1_IO01
CCM_EXT_CLK3 on GPIO1_IO06
CCM_EXT_CLK4 on GPIO1_IO07
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!