Question, i.MX8M external clock sources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX8M external clock sources

830件の閲覧回数
SLICE
Contributor IV

Dear team,

Can I understand that the external clock sources which is written in your datasheet of i.MX8M(IMX8MDQLQCEC Rev.1, 3.1.4 External clock sources) are referred to the following pins?

CCM_EXT_CLK1 GPIO1_IO00 ALT6
CCM_EXT_CLK2 GPIO1_IO01 ALT6
CCM_EXT_CLK3 GPIO1_IO06 ALT6
CCM_EXT_CLK4 GPIO1_IO07 ALT6
(From RM, IMX8MDQLQRM, Rev.0, 8.1.1.1 Muxing Options)

Regards,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

728件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Yes, the mentioned in the Datasheet(s) "four clock inputs to the CCM from normal GPIO pads via IOMUX

can be used as the clock sources in the CCM", are the following:

CCM_EXT_CLK1 on GPIO1_IO00
CCM_EXT_CLK2 on GPIO1_IO01
CCM_EXT_CLK3 on GPIO1_IO06
CCM_EXT_CLK4 on GPIO1_IO07

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信