Question, i.MX6SX CAN FIFO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX6SX CAN FIFO

跳至解决方案
1,551 次查看
SLICE
Contributor IV

Dear team,

My customer saw that sometimes i.MX6SX cannot receive CAN data from external.

The phenomenon could occur on MCIMX6SX-SDB with Yocto 4.1.15_1.1.0.

The customer believes that i.MX6SX has 6bytes of RX FIFO buffer and it needs to be exceeded.

Could you show me how to increase the RX FIFO?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 解答
1,457 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

RX FIFO is 6-deep defined by hardware and can not be changed by software,

according to sect.27.1.1 Block Diagram, sect.27.1.2 FLEXCAN Module Features i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,458 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

RX FIFO is 6-deep defined by hardware and can not be changed by software,

according to sect.27.1.1 Block Diagram, sect.27.1.2 FLEXCAN Module Features i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复