Question, i.MX6S SPDIF_SR_CLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6S SPDIF_SR_CLK

Jump to solution
2,991 Views
Aemj
Contributor IV

Hi All,

I would like to ask about SPDIF_SR_CLK on i.MX6Solo.

My customer wants to use SPDIF Rx Clock for external Codec device.

In Figure 59-2 ‘SPDIF transceiver Clock Diagram’ in i.MX6SDL reference manual, we can see SPDIF Rx Clock which is produced from SPDIF_IN flows out from DPLL.

The customer wants to use this SPDIF Rx clock for external audio codec chip.

(1)

Is it possible to output this SPDIF Rx clock from SPDIF_SR_CLK pin?

If it is not possible, do you have any ideas to output the clock from i.MX6(from other pin via other route)?

(2)

If it is possible to output the clock from i.MX, please let me know the accuracy of the clock signal.

Thanks,

Miyamoto

Labels (4)
0 Kudos
Reply
1 Solution
2,744 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Employee

Hi,

1) SPDIF Rx Clock should be equal to SPDIF_SR_CLK.

2) SPDIF Rx Clock is extracted from the SPDIF input bitstream.  That's why I said it depends on the SPDIF_IN signal.

Best regards

Raymond

View solution in original post

0 Kudos
Reply
4 Replies
2,744 Views
ShunsukeMatsuno
NXP Employee
NXP Employee

Have you read Table 59-1 in RM Rev.1?  It clearly specifies SPDIF_SR_CLK can be routed to ENET_REF_CLK pin or GPIO_8 pin.  Regarding the accuracy, it should depend on the SPDIF_IN signal.


1)
Can I understand that “SPDIF Rx Clock” is equal to “SPDIF_SR_CLK”?
If so, customer is able to output “SPDIF Rx Clock” to ENET_REF_CLK pin or GPIO_8 pin.

Answer)
SPDIF Rx Clock should be equal to SPDIF_SR_CLK.

2)
Regarding the accuracy, SPDIF Rx Clock is generated by DPLL in SPDIF Rx block. So I think the accuracy is depend on DPLL. Is my understanding correct?

Answer)
SPDIF Rx Clock is extracted from the SPDIF input bitstream.  That's why I said it depends on the SPDIF_IN signal.

0 Kudos
Reply
2,745 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Employee

Hi,

1) SPDIF Rx Clock should be equal to SPDIF_SR_CLK.

2) SPDIF Rx Clock is extracted from the SPDIF input bitstream.  That's why I said it depends on the SPDIF_IN signal.

Best regards

Raymond

0 Kudos
Reply
2,744 Views
Aemj
Contributor IV

Hi All,

Sorry for hurrying you up, but the customer needs the answer asap.

BR,

Miyamoto

0 Kudos
Reply
2,744 Views
Aemj
Contributor IV

Hi,

I am still wait for your reply.

Could you tell me the current progress status?

BR,

Miyamoto

0 Kudos
Reply