Question, i.MX6DQ PCB design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6DQ PCB design

ソリューションへジャンプ
1,313件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about PCB design for i.MX6DQ.

(1)

My customer wants to use 1005 decoupling capacitors instead of 0603 or 0201 capacitors which is written in your Hardware Design Guide of i.MX6.

Are there any problems on the use of 1005 decoupling capacitors?

(2)

In the hardware design guide(IMX6DQ6SDLHDG), 8 mils(about 0.2mm) drill is recommended. But the customer wants to use 0.15mm drill.

Are there any problems on the use of 0.15mm drill instead of 8 mils drill?

Thanks,

Miyamoto

ラベル(2)
0 件の賞賛
返信
1 解決策
1,232件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

(1) 1005 is also 0402, so the package is OK. you can use one capcitor for every 2 PADs if space is not enough.

(2)0.15mm drill is also OK.

you should pay much more attention to power net, if current is bigger, more than one drills should be used.

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,233件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

(1) 1005 is also 0402, so the package is OK. you can use one capcitor for every 2 PADs if space is not enough.

(2)0.15mm drill is also OK.

you should pay much more attention to power net, if current is bigger, more than one drills should be used.

Regards,

Weidong

0 件の賞賛
返信