Question, i.MX6 GPU specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6 GPU specification

ソリューションへジャンプ
2,305件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about i.MX6 GPU specification.

My customer wants to develop own i.MX6 GPU device driver.

Can they obtain the detailed specification of GPU 3D/2D of i.MX6?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
2,190件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Because of third-party agreement detailed information about the GPUs is not

provided. Customers should use binary libs in their applications (as is) or

apply to Freescale marketing for further considerations.

Please accept our apologies for this inconvenience.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,153件の閲覧回数
petru_l
Contributor I

Hi Yuri,

I would like to ask you in the same story, could it be feasible to request into commercial agreement the  support and instruction manual for software which direct programs the 2D GPU registers  on iMX6SX - LCDIF2 , LDB ? (from CM4 and CA9)

Thank you in advance 

Adi

0 件の賞賛
返信
2,143件の閲覧回数
Yuri
NXP Employee
NXP Employee

@petru_l 
Hello,

  The situation is still the same - it is needed to apply to NXP marketing.
 Also You may create request 

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

Regards,
Yuri.

0 件の賞賛
返信
2,191件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Because of third-party agreement detailed information about the GPUs is not

provided. Customers should use binary libs in their applications (as is) or

apply to Freescale marketing for further considerations.

Please accept our apologies for this inconvenience.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信