Question, i.MX6 GPU specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6 GPU specification

Jump to solution
2,297 Views
Aemj
Contributor IV

Dear team,

I would like to ask about i.MX6 GPU specification.

My customer wants to develop own i.MX6 GPU device driver.

Can they obtain the detailed specification of GPU 3D/2D of i.MX6?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
2,182 Views
Yuri
NXP Employee
NXP Employee

  Because of third-party agreement detailed information about the GPUs is not

provided. Customers should use binary libs in their applications (as is) or

apply to Freescale marketing for further considerations.

Please accept our apologies for this inconvenience.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,145 Views
petru_l
Contributor I

Hi Yuri,

I would like to ask you in the same story, could it be feasible to request into commercial agreement the  support and instruction manual for software which direct programs the 2D GPU registers  on iMX6SX - LCDIF2 , LDB ? (from CM4 and CA9)

Thank you in advance 

Adi

0 Kudos
Reply
2,135 Views
Yuri
NXP Employee
NXP Employee

@petru_l 
Hello,

  The situation is still the same - it is needed to apply to NXP marketing.
 Also You may create request 

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

Regards,
Yuri.

0 Kudos
Reply
2,183 Views
Yuri
NXP Employee
NXP Employee

  Because of third-party agreement detailed information about the GPUs is not

provided. Customers should use binary libs in their applications (as is) or

apply to Freescale marketing for further considerations.

Please accept our apologies for this inconvenience.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply