Question, i.MX25 BT_SPARE_SIZ setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX25 BT_SPARE_SIZ setting

跳至解决方案
1,163 次查看
Aemj
Contributor IV

Dear team,

I would like to ask about BT_SPARE_SIZ setting of i.MX25.

On my customer’s i.MX25 board, NAND-flash which has page-size of 512Byte is used for Boot storage.

i.MX25 does not boot-up when they set BT_SPARE_SIZ to 218B.

And when they set BT_SPARE_SIZ to 128B, then i.MX25 can boot-up.

Is setting BT_SPARE_SIZ reasonable for 512B pagesize NAND?

Could you show me what BT_SPARE_SIZ should be set to for 512b pagesize NAND?

And please let me know BT_SPARE_SIZ setting for 2KB NAND as well.

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 解答
1,086 次查看
Yuri
NXP Employee
NXP Employee

  Please refer to Table 3 (Fuse Descriptions) of the app note AN3684, regarding

using the spare size parameter :

BT_SPARE_SIZE - Specifies the size of spare bytes for 4 Kbyte page size NAND

Flash devices.

Note: 512 byte page devices have 16 bytes spare area size,

2 Kbyte page devices have 64 bytes spare area size.

Note: Assumes that the large spare area devices (218 byte) use 8-bit ECC.

Otherwise, 4-bit ECC.

< http://cache.freescale.com/files/dsp/doc/app_note/AN3684.pdf >

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,087 次查看
Yuri
NXP Employee
NXP Employee

  Please refer to Table 3 (Fuse Descriptions) of the app note AN3684, regarding

using the spare size parameter :

BT_SPARE_SIZE - Specifies the size of spare bytes for 4 Kbyte page size NAND

Flash devices.

Note: 512 byte page devices have 16 bytes spare area size,

2 Kbyte page devices have 64 bytes spare area size.

Note: Assumes that the large spare area devices (218 byte) use 8-bit ECC.

Otherwise, 4-bit ECC.

< http://cache.freescale.com/files/dsp/doc/app_note/AN3684.pdf >

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,086 次查看
Aemj
Contributor IV

Dear Yuri,

Thanks for your reply.

Can I understand that BT_SPARE_SIZE must be 0(128B) for 512B and 2KB pagesize NAND?

Best Regards,

Miyamoto

0 项奖励
回复
1,086 次查看
Yuri
NXP Employee
NXP Employee

Correct - "BT_SPARE_SIZE must be 0(128B) for 512B and 2KB pagesize NAND".

~Yuri.

0 项奖励
回复