Question, i.MX25 32K clock input.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX25 32K clock input.

ソリューションへジャンプ
1,400件の閲覧回数
Aemj
Contributor IV

Dear team,

My customer plans to use 32K crystal for i.MX25 OSC32K_EXTAL.

On their board, the 32K clock input from the crystal can be stable at 500mS later after the release of POR.

Is it OK?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,308件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

       Actually, the 32K clock should be stable before POR releases, because after POR , ROM code will use the clock to do booting configurations.

       But according to the customer's issue, if system is not stable, she can consider delaying the time of POR over 500ms !

       Hope the suggestion can help you !

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,309件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

       Actually, the 32K clock should be stable before POR releases, because after POR , ROM code will use the clock to do booting configurations.

       But according to the customer's issue, if system is not stable, she can consider delaying the time of POR over 500ms !

       Hope the suggestion can help you !

Regards,

Weidong

0 件の賞賛
返信