Question, i.MX25 32K clock input.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX25 32K clock input.

Jump to solution
1,390 Views
Aemj
Contributor IV

Dear team,

My customer plans to use 32K crystal for i.MX25 OSC32K_EXTAL.

On their board, the 32K clock input from the crystal can be stable at 500mS later after the release of POR.

Is it OK?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
1,298 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

       Actually, the 32K clock should be stable before POR releases, because after POR , ROM code will use the clock to do booting configurations.

       But according to the customer's issue, if system is not stable, she can consider delaying the time of POR over 500ms !

       Hope the suggestion can help you !

Regards,

Weidong

View solution in original post

0 Kudos
Reply
1 Reply
1,299 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

       Actually, the 32K clock should be stable before POR releases, because after POR , ROM code will use the clock to do booting configurations.

       But according to the customer's issue, if system is not stable, she can consider delaying the time of POR over 500ms !

       Hope the suggestion can help you !

Regards,

Weidong

0 Kudos
Reply