Question about i.MX8QXP Startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about i.MX8QXP Startup

ソリューションへジャンプ
2,257件の閲覧回数
jiangpengfei
Contributor I

Hi, buddies:

I've got an issue when start up Linux kernel from u-boot. The description of the issue is following, and you can find the u-boot log in attachment:

1. We use uuu download bootloader to the customized board, the bootloader includes SCFW, SECO FW, m4 image and u-boot image;

2. We download Linux kernel and binary device tree to memory through ethernet;

3. We use booti command to startup kernel, but the system is stuck at Starting kernel ...

We can't find any clue to this issue, but it looks like none of code of kernel is executed at the moment. (We tried to modify the value of memory address "0x88000000" in "start_kernel" function in kernel, but the value wasn't changed when we verified the value in SCFW console).


We hope NXP technical support can give us some advice about how to solve this issue.

Thanks a lot!

0 件の賞賛
返信
1 解決策
2,096件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Jiang,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,097件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Jiang,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,096件の閲覧回数
jiangpengfei
Contributor I

Hi, CarlosCasillas:

Thanks for your information, it's useful for us.

We've already contack our FAE, they haven't yet replied.

We'll ask them again today.

0 件の賞賛
返信