Question about VPU EncOpenParam

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about VPU EncOpenParam

ソリューションへジャンプ
2,653件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

 

 

Let me ask about a EncOpenParam for VPU operation.

 

Q1.

If EncOpenParam's bitRate is set to something other than "0", will it exceed the specified bitRate?

* Will it be controlled at a fixed bit rate?

 

Q2.

If EncOpenParam's bitRate is specified with something other than "0", will it compensate to the specified bit rate with padding when the bit rate is less than the bit rate specified at encoding?

 

Q3.

Does userOpMax and userQpMin set the fluctuation range of the Q value in units of macroblocks?

 

 

Ko-hey

0 件の賞賛
返信
1 解決策
2,494件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for bitrate, which depends on what mode you use, if you use CBR, yes, you can set the fixed bitrate

what do you mean userOpMax  and Q value? do you mean QP value?

if yes, refer to the VPU  API reference manual, pMBQpInfo is not used in imx6

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,494件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Could someone follow and answer this thread ?

Ko-hey

0 件の賞賛
返信
2,495件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for bitrate, which depends on what mode you use, if you use CBR, yes, you can set the fixed bitrate

what do you mean userOpMax  and Q value? do you mean QP value?

if yes, refer to the VPU  API reference manual, pMBQpInfo is not used in imx6

0 件の賞賛
返信