Question about PCIe Validation hardware setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about PCIe Validation hardware setup

跳至解决方案
1,416 次查看
ko-hey
Senior Contributor II

Hi all

Let me ask about the following thread, especially cable and bridge board.

i.MX6Q PCIe EP/RC Validation System 

My customer plan to emulate the PCIe EP/RC and are finding the bridge board.

Finally, they found the following validation system and want to use the boards which are surrounded by red circle selling.

bridgeboard.jpg

Q1.

Are the boards which are surrounded by red circle selling ?

Q2.

And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Ko-hey

标签 (2)
0 项奖励
回复
1 解答
1,323 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,324 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,323 次查看
ko-hey
Senior Contributor II

Hi wigros.sun wigros.sun

Thank you for advice.

I'll talk with customer.

Ko-hey

0 项奖励
回复