Question about PCIe Validation hardware setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about PCIe Validation hardware setup

ソリューションへジャンプ
2,237件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Let me ask about the following thread, especially cable and bridge board.

i.MX6Q PCIe EP/RC Validation System 

My customer plan to emulate the PCIe EP/RC and are finding the bridge board.

Finally, they found the following validation system and want to use the boards which are surrounded by red circle selling.

bridgeboard.jpg

Q1.

Are the boards which are surrounded by red circle selling ?

Q2.

And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Ko-hey

ラベル(2)
0 件の賞賛
返信
1 解決策
2,144件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,145件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,144件の閲覧回数
ko-hey
Senior Contributor II

Hi wigros.sun wigros.sun

Thank you for advice.

I'll talk with customer.

Ko-hey

0 件の賞賛
返信