Question about PCIe Validation hardware setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about PCIe Validation hardware setup

Jump to solution
1,369 Views
ko-hey
Senior Contributor II

Hi all

Let me ask about the following thread, especially cable and bridge board.

i.MX6Q PCIe EP/RC Validation System 

My customer plan to emulate the PCIe EP/RC and are finding the bridge board.

Finally, they found the following validation system and want to use the boards which are surrounded by red circle selling.

bridgeboard.jpg

Q1.

Are the boards which are surrounded by red circle selling ?

Q2.

And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Ko-hey

Labels (2)
0 Kudos
Reply
1 Solution
1,276 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,277 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello  Ko-hey

>>Are the boards which are surrounded by red circle selling ?

 No, they are not. both cards are only used for R&D.

>>And the cable is as below. Am I correct ?

External PCI Express (PCIe) - Molex 

Yes, you are right.

In additon, my advicde for you:

  Because PCIe signals are conneted to MiniPCIe connector on SabreSDP / SDB board, probably it is not convenient for customer to test PCIe communication, customer can design a simple Conversion Card with MiniPCIe interface, see following diagram:

pastedImage_1.png


Have a great day,
Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,276 Views
ko-hey
Senior Contributor II

Hi wigros.sun wigros.sun

Thank you for advice.

I'll talk with customer.

Ko-hey

0 Kudos
Reply