Question about CCM_CACRR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about CCM_CACRR

Jump to solution
1,706 Views
宗標廖
Contributor V

Hello Community

In page 829 of imx6sdl reference manual(IMX6SDLRM.pdf Rev.2),there is description for arm_podf in CCM_CACRR as bellow.

--------------

NOTE: If arm_freq_shift_divider is set to '1' then any new write to arm_podf will be held until
arm_clk_switch_req signal is asserted.

--------------

I searched arm_freq_shift_divider and arm_clk_switch_req in IMX6SDLRM.pdf, buf cannot find them in anywhere else.

So what does this NOTE mean?

Thank you!

ZongbiaoLiao

Labels (4)
0 Kudos
Reply
1 Solution
1,616 Views
Yuri
NXP Employee
NXP Employee

Hello

  This relates to bit “arm_podf_busy” of CCM Divider Handshake In-Process Register (CCM_CDHIPR) :

 

Busy indicator for “arm_podf”.


0 - divider is not busy and its value represents the actual division.


1 - divider is busy with handshake process with module. The value read in the divider represents the previous

value of the division factor, and after the handshake the written value of the arm_podf will be applied.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
Reply
1 Reply
1,617 Views
Yuri
NXP Employee
NXP Employee

Hello

  This relates to bit “arm_podf_busy” of CCM Divider Handshake In-Process Register (CCM_CDHIPR) :

 

Busy indicator for “arm_podf”.


0 - divider is not busy and its value represents the actual division.


1 - divider is busy with handshake process with module. The value read in the divider represents the previous

value of the division factor, and after the handshake the written value of the arm_podf will be applied.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply