TrustZone support in WaRP7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TrustZone support in WaRP7

1,460件の閲覧回数
iancarroll
Contributor I

Hi,

Is it possible to take advantage of TrustZone on the WaRP7? Additionally, is there support for the iMX 7 CAAM module and/or secure volatile storage (SNVS)? 

ラベル(1)
0 件の賞賛
返信
1 返信

1,245件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ian

please check attached Linux Manual Chapter 50 CAAM

and examples in imx-test package (../test/caam)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

there is no special trustzone support in nxp bsps and one can look at

"Normal world" Linux for iMX6Q Lite 

ARM Information Center 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信