Query regarding the sampling rate of BCU utility for power measurements on iMX93EVK board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query regarding the sampling rate of BCU utility for power measurements on iMX93EVK board

553 Views
Vikas7Bal
Contributor II

Hi,

I am trying to perform power measurements on the iMX93EVK board using the host based BCU utility.

I have observed that, the BCU sampling rate is fixed at 10 ms and from the BCU.pdf I came to know that "BCU operates at best sampling rate possible" and I couldn't find a way to configure the sampling rate.

So, is it possible to configure the sampling rate for BCU?

Also, in the nxp-imx/bcu git repo which is used to build the utility, I observed that, "MAX_NUMBER_OF_POWER" macro is being hardcoded to 100 which could probably be the reason for 10 ms sampling rate.

So is it possible to change it to higher values so that I can build the tool from the source code and achieve much finer sampling rate?

Labels (1)
0 Kudos
Reply
1 Reply

475 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello @Vikas7Bal 

The sampling rate is hardcoded with many other code in BCU, modifing it in source code could cause other compatible issue. We don't recommend you modify it.


Best Regards,
Zhiming

0 Kudos
Reply