Query on i.MX6Q IBIS model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query on i.MX6Q IBIS model

Jump to solution
1,586 Views
anandmeharwade
Contributor II


Hi

I have downloaded the IBIS model for i.MX6Q and I want to simulate for SATA, PCIe signals. I am Observing that the SATA and PCIe TX diff pairs are assigned as inputs. In this case how can I use the i.Mx6q as driver to transmit the bit pattern

Could you please clarify on this

Thanks

Anand M

Labels (1)
0 Kudos
Reply
1 Solution
1,487 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anand

some pins are not covered by ibis model, as described in Table 9-6. i.MX6 pins not supported by IBIS

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,488 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anand

some pins are not covered by ibis model, as described in Table 9-6. i.MX6 pins not supported by IBIS

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply