power off a battery-less device by removing power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

power off a battery-less device by removing power

355 Views
dty2015
Contributor I

HI, There,

We have a device that does not have a battery. It seems that it can be shut down by removing power and reboot every time. The Android is Lollipop on a Sabre-based platform. Two questions.

1. The question is does Android or Linux has file system. What is the mechanism to make reboot successfully since removing power is like abnormal shutdown?

2. Would be any chance that the system will not boot up properly?

Many thanks for your looking and providing meaning answer.

DTY

0 Kudos
1 Reply

307 Views
igorpadykov
NXP Employee
NXP Employee

HI Dale

yes both have filesystems. In general it is necessary to power off

device using methods suggested by used OS, for example poweroff

in linux, so current filesystem operations could be finished safely by OS.

If file system is damaged during sudden removing power, next time it

could fail to boot.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos