Query on SC16IS750IBS (RS232, RS485 Controller I²C, SPI, UART Interface)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query on SC16IS750IBS (RS232, RS485 Controller I²C, SPI, UART Interface)

751 Views
manumathew
Contributor I

We had a query on SC16IS750IBS.

 

We would like to know if the GPIO0 pin of this device defaults to an input on power up?

Labels (1)
0 Kudos
Reply
1 Reply

700 Views
b36401
NXP Employee
NXP Employee

Yes. They are inputs on power up.

  

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply