i.MX6 TW6869 driver source code for Linux L4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 TW6869 driver source code for Linux L4.1.15

1,867 Views
waynekuo
Contributor III

Hi everyone,

Do NXP provide the driver source code of TW6869 on Linux L4.1.15?

I found a community thread provide the patch for L3.10.53 and L3.14.48.

How to pass DMA buffers from a Driver thru GStreamer 'v4l2src' plugin to Freescale IPU/VPU plugins 

Does these patches works on L4.1.15?

How can I get the source code of TW6869?

Any information / suggestion is helpful. Thank you.

Best Regrds,

Wayne Kuo

0 Kudos
Reply
1 Reply

1,329 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wayne

sorry it is not supported in official nxp bsps, supported drivers can be

found in documentation (Release Notes) on link

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


================================================================
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply