Query on HAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query on HAB

1,511件の閲覧回数
Maheshkadam9922
Contributor II

we have one query below

suppose we flash the signed or encrypted image image on mxrt1050 evk board using secure provisioning tool after then can we debug the code using MCUxpesso tool ?.

we have only one board so one development team working on CAN code , so they need to debug code using MCUxpresso tool 

we also show the demo of HAB signed image .

actually our plan to flash the CAN code using secure tool with activate signed (HAB) feature and debug this code using MCUXpresso tool

 

 

 

 

 

 

 

 

 

0 件の賞賛
返信
2 返答(返信)

1,474件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Maheshkadam9922 

Whether it can be debugged has nothing to do with the signature or encryption of the image itself. e.g., JLINK tool.  As long as it is debugged in the attach mode and JTAG is not disabled, it can be debugged.

 

Best regards

Harvey

0 件の賞賛
返信

1,498件の閲覧回数
Maheshkadam9922
Contributor II

Our development team is currently working on CAN code for the MXRT1050 EVK board and we want flash a signed or encrypted image using the secure provisioning tool, which activates the High Assurance Boot (HAB) feature.

However, we would like to inquire about the possibility of debugging the same code using the MCUxpresso tool after flashing the HAB-signed image using secure provisioning tool. Since we only have one board available, Can our development team to be able to debug the CAN code using the familiar MCUxpresso tool after flashing CAN code with the HAB-signed image using secure provisioning tool?

Could you kindly confirm whether it is possible to debug the code using the MCUxpresso tool after flashing a HAB-signed image?

0 件の賞賛
返信