Quad SPI availability with iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quad SPI availability with iMX6

Jump to solution
8,215 Views
Poussemousse
Contributor III

Hello,

I would like to know if there is any possibility to have a Quad SPI (or QSPI) interface with an iMX6Solo in order to have a faster access to SPI NOR.

The datasheet offers 2 single data standard SPI interface with 4 chip select pins,

and several SDIO interfaces with 4 to 8 bits data bus width.

In the SABRE Platform for IPTV based on i.MX 6  Block Diagram

2 QSPI are mentionned but nothing else.

Does anyone could confirm if it is possible to have a Quad SPI interface ?

Thanls for your help,

Regards.

Pousssemousse

0 Kudos
Reply
1 Solution
5,680 Views
Clay_Turner
NXP Employee
NXP Employee

The current i.MX6 products (6Quad, 6Dual, 6DualLite, 6Solo and 6SoloLite) do not support QSPI. This appears to be an error in the presentation.

Regards,

Clay

View solution in original post

0 Kudos
Reply
8 Replies
5,680 Views
Poussemousse
Contributor III

According Freescale news :

http://media.freescale.com/phoenix.zhtml?c=196520&p=irol-newsArticle&ID=1917475&highlight=

iMX6SoloX will provide the feature plus :

Additional features of the newest i.MX 6 series processor include:

  • Dual-port gigabit Ethernet audio video bridging (AVB) for quality-of-service in automotive and other applications with enhanced traffic shaping and packet prioritization.
  • Cost-effective 2D and 3D graphics processing unit (GPU) for enhanced HMI development.
  • Flexible boot options, including support for quad SPI and raw NAND, and a memory controller that interfaces to both DDR3 and low power DDR2.
0 Kudos
Reply
5,681 Views
Clay_Turner
NXP Employee
NXP Employee

The current i.MX6 products (6Quad, 6Dual, 6DualLite, 6Solo and 6SoloLite) do not support QSPI. This appears to be an error in the presentation.

Regards,

Clay

0 Kudos
Reply
5,680 Views
Poussemousse
Contributor III

Bruce or Clay ??

Thanks for this clarification. Do you expect to have a future firmware revision with Quad SPI integrated in the chip ?

Starting from USDHC peripheral should not be too complicated to offer a Quad SPI bus to your customers.

Regards

Poussemousse.

0 Kudos
Reply
5,680 Views
Clay_Turner
NXP Employee
NXP Employee

Yes. A future chip will have a dedicated Quad SPI peripheral (implemented in hardware not in firmware through another interface).

Regards,

Clay

0 Kudos
Reply
5,680 Views
Poussemousse
Contributor III

Will this chip be pin to pin compatible with current iMX6,

and when do you expect to propose such component ?

0 Kudos
Reply
5,680 Views
Clay_Turner
NXP Employee
NXP Employee

Unfortunately, I can't provide details about unannounced products.

Regards,

Clay

0 Kudos
Reply
5,680 Views
fabio_estevam
NXP Employee
NXP Employee

Vybrid is an announced Freescale product that supports QuadSPI.

Driver has alreadby been submitted:

[PATCH v3 0/8] Add the Quadspi driver for vf610-twr (Linux Doc)

0 Kudos
Reply
5,680 Views
fabio_estevam
NXP Employee
NXP Employee

As per described in the mx6 solo reference manual, it contains the standard ECSPI block.