Hello,
I would like to know if there is any possibility to have a Quad SPI (or QSPI) interface with an iMX6Solo in order to have a faster access to SPI NOR.
The datasheet offers 2 single data standard SPI interface with 4 chip select pins,
and several SDIO interfaces with 4 to 8 bits data bus width.
In the SABRE Platform for IPTV based on i.MX 6 Block Diagram
2 QSPI are mentionned but nothing else.
Does anyone could confirm if it is possible to have a Quad SPI interface ?
Thanls for your help,
Regards.
Pousssemousse