Qt5MultimediaWidget

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qt5MultimediaWidget

1,992件の閲覧回数
强王
Contributor IV

目前我们使用3.10.53 yocto

如下步骤下载代码:

source setup-environment

MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-fb -e fb

bitbake fsl-image-qt5

编译好的ROOTFS包里面没有Qt5MultimediaWidget库,

然后我们手动编译Qt5MultimediaWidget这个库进去

运行代码:报错红色字体

./player  -platform eglfs

QEglFSImx6Hooks will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.

If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

EGLFS: Unable to query physical screen size, defaulting to 100 dpi.

EGLFS: To override, set QT_QPA_EGLFS_PHYSICAL_WIDTH and QT_QPA_EGLFS_PHYSICAL_HEIGHT (in millimeters).

defaultServiceProvider::requestService(): no service found for - "org.qt-project.qt.mediaplayer"

This plugin does not support propagateS

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,702件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

For the fsl-image-qt5 the backend to use is x11 not fb. Please try that and let me know how it goes.

Best Regards,

Alejandro

0 件の賞賛
返信