yocto display unnormal on the arm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto display unnormal on the arm

1,185 Views
俊宝胡
Contributor I

Hello, I use i.MX6qsabresd platform and fsl-yocto-3.14.28 BSP

I use a lvds screen on the imx6qsabresd borad.

I input the following command

(1)MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb

(2)Edit yocto/build/conf/bblayers.conf to add the meta-qt5 layer at the end:

${BSPDIR}/sources/meta-qt5 \

${BSPDIR}/sources/meta-openembedded/meta-ruby \

${BSPDIR}/sources/meta-openembedded/meta-multimedia \

(3)Edit yocto/build/conf/local.conf

  EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh "

  IMAGE_INSTALL_append = " gcc g++ binutils libgcc libgcc-dev libstdc++ libstdc++-dev libstdc++-staticdev \

  autoconf automake ccache chkconfig glib-networking glibmm \

  packagegroup-core-buildessential pkgconfig  \

  boost cmake zlib glib-2.0 packagegroup-fsl-tools-testapps  \

    ruby \

    cpufrequtils \

    nano \

    gdb \

    gstreamer \

    gst-meta-video \

    gst-fsl-plugin \

    gst-plugins-base-app \

    gst-plugins-base \

    gst-plugins-good \

    gst-plugins-good-rtsp \

    gst-plugins-good-udp \

    gst-plugins-good-rtpmanager \

    gst-plugins-good-rtp \

    gst-plugins-good-video4linux2 \

    openssh-sftp-server \

    packagegroup-fsl-gstreamer \

    packagegroup-fsl-tools-testapps \

    packagegroup-fsl-tools-benchmark \

    imx-vpu \

    imx-test \   

    qtbase-fonts \

    qtbase-plugins \

    qtbase-tools \

    qtbase-examples \

    qtdeclarative \

    qtdeclarative-plugins \

    qtdeclarative-tools \

    qtdeclarative-examples \

    qtdeclarative-qmlplugins \

    qtmultimedia \

    qtmultimedia-plugins \

    qtmultimedia-examples \

    qtmultimedia-qmlplugins \

    qtsvg \

    qtsvg-plugins \

    qtsensors \

    qtimageformats-plugins \

    qtsystems \

    qtsystems-tools \

    qtsystems-examples \

    qtsystems-qmlplugins \

    qtscript \

    qt3d \

    qt3d-examples \

    qt3d-qmlplugins \

    qt3d-tools \

    qtwebkit \

    qtwebkit-examples-examples \

    qtwebkit-qmlplugins \

    qtgraphicaleffects-qmlplugins \

    qtconnectivity-qmlplugins \

    qtlocation-plugins \

    qtlocation-qmlplugins \

    cinematicexperience \

    cairo pango fontconfig freetype pulseaudio dbus \

    alsa-lib alsa-tools alsa-state alsa-utils-alsaconf fsl-alsa-plugins \

    i2c-tools \

    "

  DISTRO_FEATURES_remove = "x11 wayland"

(4bitbake fsl-image-qt5

builds was successfull,I flash the rootfs.tar.gz on the arm board,can display Yocto Project,

but can't display any on the screen,like this command: cat wall-1024x768-565.rgb  > /dev/fb0

I found My QT5 only support as below:

Available platform plugins are: minimal, offscreen, wayland, wayland-xcomposite-egl, xcb

Also can not display qt5 examples

help me ,thanks.

0 Kudos
Reply
1 Reply

928 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello yiyi521,

I’m sorry to hear you’re having troubles with the QT5 image. Have you tried using X11 as backend? QT5 requires this backend in order to work properly. That is very likely at least part of the problem.

Let us know of your findings!

0 Kudos
Reply