QWKS-SCM-IMX6DQ schematic clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QWKS-SCM-IMX6DQ schematic clarification

Jump to solution
4,676 Views
sunjianxin66
Contributor II

Dear NXP

I am looking at the QWKS-SCM-IMX6DQ, Quick Start Board for SCM-i.MX 6DQ, and found on Page 7 PMIC Control block. It says 

PMIC_VDDOTP
1.5V = PMIC boots from default.
0 = PMIC boots from OTP fuse map.
R42 works with the internal 10k pulldown to provide 1.5V
to PMIC_VDDOTP. R42, R43 & C28 are not needed if
using OTP fuse map.

This is inconsistent with the schematic. Could you please help clarify this? Thank you very much! Schematic and screen shoot attached. 

Jianxin

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,389 Views
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

View solution in original post

0 Kudos
Reply
3 Replies
4,389 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi JIANXIN,

You are rigth, however the R42 should be pull up, and the R43 and C28 are not need it if using OTP.

0 Kudos
Reply
4,390 Views
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

0 Kudos
Reply
4,389 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct!!

0 Kudos
Reply