QWKS-SCM-IMX6DQ schematic clarification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QWKS-SCM-IMX6DQ schematic clarification

跳至解决方案
4,713 次查看
sunjianxin66
Contributor II

Dear NXP

I am looking at the QWKS-SCM-IMX6DQ, Quick Start Board for SCM-i.MX 6DQ, and found on Page 7 PMIC Control block. It says 

PMIC_VDDOTP
1.5V = PMIC boots from default.
0 = PMIC boots from OTP fuse map.
R42 works with the internal 10k pulldown to provide 1.5V
to PMIC_VDDOTP. R42, R43 & C28 are not needed if
using OTP fuse map.

This is inconsistent with the schematic. Could you please help clarify this? Thank you very much! Schematic and screen shoot attached. 

Jianxin

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,426 次查看
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,426 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi JIANXIN,

You are rigth, however the R42 should be pull up, and the R43 and C28 are not need it if using OTP.

0 项奖励
回复
4,427 次查看
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

0 项奖励
回复
4,426 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct!!

0 项奖励
回复