QWKS-SCM-IMX6DQ schematic clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QWKS-SCM-IMX6DQ schematic clarification

ソリューションへジャンプ
4,716件の閲覧回数
sunjianxin66
Contributor II

Dear NXP

I am looking at the QWKS-SCM-IMX6DQ, Quick Start Board for SCM-i.MX 6DQ, and found on Page 7 PMIC Control block. It says 

PMIC_VDDOTP
1.5V = PMIC boots from default.
0 = PMIC boots from OTP fuse map.
R42 works with the internal 10k pulldown to provide 1.5V
to PMIC_VDDOTP. R42, R43 & C28 are not needed if
using OTP fuse map.

This is inconsistent with the schematic. Could you please help clarify this? Thank you very much! Schematic and screen shoot attached. 

Jianxin

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,429件の閲覧回数
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,429件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi JIANXIN,

You are rigth, however the R42 should be pull up, and the R43 and C28 are not need it if using OTP.

0 件の賞賛
返信
4,430件の閲覧回数
sunjianxin66
Contributor II

Thanks for the reply

Just confirm, are the R42, R43 and C28 mentioned in the green color paragraph should be R47, R48 and C38 in the schematic connection?

Thank you. 

Jianxin

0 件の賞賛
返信
4,429件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct!!

0 件の賞賛
返信