Python-Opencv based on Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Python-Opencv based on Yocto

ソリューションへジャンプ
6,986件の閲覧回数
nurulhidayah
Contributor I

I'm currently working on a project related to python programming.

I need to use python-openCV for the project, which will later run in I.MX6 board.

So, I will need to bind the prebuild openCV package in Yocto to python (not C/C++)

How can it be done in Yocto?

Because usually, python-openCv and openCv will give different library when installed in computer.

Fyi, the image i'm building is the core-image-weston.

ラベル(3)
0 件の賞賛
返信
1 解決策
4,981件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to

Install python-opencv module 

opencv 3.1 supports on the mx6q board
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,982件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to

Install python-opencv module 

opencv 3.1 supports on the mx6q board
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信