Python-Opencv based on Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Python-Opencv based on Yocto

跳至解决方案
6,059 次查看
nurulhidayah
Contributor I

I'm currently working on a project related to python programming.

I need to use python-openCV for the project, which will later run in I.MX6 board.

So, I will need to bind the prebuild openCV package in Yocto to python (not C/C++)

How can it be done in Yocto?

Because usually, python-openCv and openCv will give different library when installed in computer.

Fyi, the image i'm building is the core-image-weston.

标签 (3)
0 项奖励
回复
1 解答
4,054 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to

Install python-opencv module 

opencv 3.1 supports on the mx6q board
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
4,055 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to

Install python-opencv module 

opencv 3.1 supports on the mx6q board
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复