Pulse width between two chip select of SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pulse width between two chip select of SPI

Jump to solution
1,474 Views
daweiyou
NXP Employee
NXP Employee

Hi Guys:

Here are question for Pulse width between two chip select of SPI, i.MX6

The Wait States between two Chip Select (SS) signals can be decided

by ECSPI_PERIODREG[SAMPLE_PERIOD], but even if SAMPLE_PERIOD is 0,

the wait width still exist, from datasheet, the Min of "CS4 ECSPIx_SSx pulse width", tCSLH , is Half ECSPIx_SCLK period,

but Max is not defined.

So could you tell me what's the Max value and how to adjust it?

Actually, by testing, the actual value is almost 1us, if I want to reduce it, how can I do? thx

0 Kudos
Reply
1 Solution
1,265 Views
YixingKong
Senior Contributor IV

Dawei

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

View solution in original post

0 Kudos
Reply
1 Reply
1,266 Views
YixingKong
Senior Contributor IV

Dawei

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply