Prototyping board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Prototyping board

Jump to solution
3,200 Views
mouha
Contributor I

Hi,

I'm a Linux embedded developer who already own some board like the mini2440, or TS7260.

I'm new here, and admit to be lost about the i.MX53 which seems to be great :

- what board do I need to easily go prototyping when I see the freescale devboard but also a iWave Q7 one : does it means that the Devboard is not enough to get connectors  (GPIO, Ethernet, Sata, etc) and to power it ? in other words : what advice to choose a protyping board ?

- according to the numerous document Linux  (not Android) is easily provided for this board but how far when I want to access to accelermoter ?

DL

Labels (1)
0 Kudos
Reply
1 Solution
3,123 Views
hippo
NXP TechSupport
NXP TechSupport

We have two reference designs based on i.mx53. One is i.mx53QSB, the other one is SABRE for tablets. And SABRE is discounted to $999 now.

Please see the comparison table of these two boards.

SABRE for tablets vs. QSB - Comparison.JPG

View solution in original post

0 Kudos
Reply
2 Replies
3,124 Views
hippo
NXP TechSupport
NXP TechSupport

We have two reference designs based on i.mx53. One is i.mx53QSB, the other one is SABRE for tablets. And SABRE is discounted to $999 now.

Please see the comparison table of these two boards.

SABRE for tablets vs. QSB - Comparison.JPG

0 Kudos
Reply
3,123 Views
mouha
Contributor I

Thank you for the answer, even though I wonder almost between IMX53QSB (quick start board) and iWave Q7

as ignore if the QSB is enough to be used as is: just with the board and no additional connectors or adaptation to use it.

0 Kudos
Reply