Programming eMMC from user space

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming eMMC from user space

ソリューションへジャンプ
2,928件の閲覧回数
eren_yilmaz
Contributor III

Is there a way of accessing eMMC to replace the u-boot image, the device-tree etc. from user space?

The only tool I could find is mmc-utils and it does not allow erasing or writing on the flash.

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,837件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eren

one can check

How to upgrade Linux Kernel and dtb on eMMC without UUU  

https://boundarydevices.com/programming-emmc-on-i-mx6/ 

Mfg Tool scripts (ucl2.xml) on link i.MX Software and Development Tools | NXP 

Mfg Tool is running small linux image and scripts are used for programming external memories.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eren

one can check

How to upgrade Linux Kernel and dtb on eMMC without UUU  

https://boundarydevices.com/programming-emmc-on-i-mx6/ 

Mfg Tool scripts (ucl2.xml) on link i.MX Software and Development Tools | NXP 

Mfg Tool is running small linux image and scripts are used for programming external memories.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------