I got a MXIMX8m-EVKB Board .
And I want to update all (not only kernel)the latest fireware for it
After downlading the L4.19.35_1.1.0_MX8MQ , which file is for MXIMX8m-EVKB Board
I had check the document i.MX_Linux_User's_Guide.
would anyone give an example for this ?
Hello,
The uboot binary present on the L4.19.35_1.1.0_MX8MQ by default is the following:
imx-boot-imx8mqevk-sd.bin-flash_evk
You may flash this uboot binary for SD or eMMC, to update your firmware please follow the step in the i.MX Linux User's Guide section 4.2 Universal update utility.
Hope this helps,
Regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------