Programm SPI interface for imx6s android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programm SPI interface for imx6s android

2,151件の閲覧回数
androidimx6s
Contributor I

How to configure SPI interface for android. Shall we write application using c/cpp ?

Is there any inbuilt driver design for SPI which we can used to open SPI port and configure the SPI port?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,017件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

ECSPI driver implements a standard Linux driver interface (android is based on linux)

please refer to Chapter 36 Enhanced Configurable Serial Peripheral Interface (ECSPI) Driver

attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信