Issue uboot console not display on screen android kitkat 4.4.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue uboot console not display on screen android kitkat 4.4.

2,030 次查看
dipakdesai
Contributor I

Imx6q board connect with register touch screen. It is working good. Now i want to used LCD capacities touch screen but did display did not work. I found that require to change boot environment, but i did not able to enter uboot>  console. OS used is kitkat 4.4.

标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

1,913 次查看
b36401
NXP Employee
NXP Employee

Please note that this command prompt appears not on a graphic display attached to i.MX but on the terminal connected to UART.
You need to connect PC to "debug UART" port of i.MX board and run virtual terminal on this PC.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,913 次查看
dipakdesai
Contributor I

Thanks to reply. 

I came to know that console is disable, So, Is there other way to enable boot configuration? 

0 项奖励
回复