Profiles imx 35 for application mgftool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Profiles imx 35 for application mgftool

990 次查看
nico70
Contributor I

Hello,

I use application mfgtool with the imx35 but the problem is to realize the application profile for the imx 35, that does not exist in my version.

My objective is to download an image in the NAND flash of my platform.

I search an example or a profile for this imx35 for MFGTOOL

Nico

标记 (4)
0 项奖励
回复
1 回复

846 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Nicolas,

The i.MX35 does not use the MFGTool, it instead uses ATK (Advanced ToolKit), you can download it from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX353&nodeId=018rH3ZrDR633D&fpsp=1&...

Under: Hardware Development Tools --> Programmers --> IMX_ADVANCEDTOOLKIT

0 项奖励
回复