Profiles imx 35 for application mgftool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Profiles imx 35 for application mgftool

1,365 Views
nico70
Contributor I

Hello,

I use application mfgtool with the imx35 but the problem is to realize the application profile for the imx 35, that does not exist in my version.

My objective is to download an image in the NAND flash of my platform.

I search an example or a profile for this imx35 for MFGTOOL

Nico

Tags (4)
0 Kudos
Reply
1 Reply

1,221 Views
SergioSolis
NXP Employee
NXP Employee

Hello Nicolas,

The i.MX35 does not use the MFGTool, it instead uses ATK (Advanced ToolKit), you can download it from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX353&nodeId=018rH3ZrDR633D&fpsp=1&...

Under: Hardware Development Tools --> Programmers --> IMX_ADVANCEDTOOLKIT

0 Kudos
Reply