Procedure to apply Patch for Kernel(2.6.35) in Ltib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Procedure to apply Patch for Kernel(2.6.35) in Ltib

2,608 Views
santhoshkarthik
Contributor III

Hi,

   I am using Linux 2.6.35.03 kernel. I am working on FlexCAN. I had installed "canutils" and "libsocket". But i am not able to set the bitrate with following command

 

ip link set can0 type can bitrate 125000

it was showing following error

RTNETLINK answers: operation not supported

 

I posted the query and I got patch from the Community. Could you please tell me the procedure to apply patch for kernel

I have attached the patch

Original Attachment has been moved to: linux-2.6.35_mainline_flexcan.patch.zip

Labels (1)
1 Reply

2,337 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karthikeyan

https://community.nxp.com/thread/299202 

also for general procedure applying patches please refer to attached document

p.3 from L2.6.35_11.09 documentation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------