Problems with GPU process crashing in Chromium

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with GPU process crashing in Chromium

3,767件の閲覧回数
IanCraig
Contributor II

Hi

I'm trying to get Chromium running on the SabreSD board and having problems with the GPU process crashing when opening a web page. My setup is as follows

FSL Community BSP 1.8 Fido

Kernel 3.14.28-1.0.0_ga+g91cf351

core-image-sato image with chromium (40.0.2214.91) added

Freescale SabreSD board

On boot chromium reports hardware acceleration is enabled and everything looks fine but as soon as you open a web page and check chrome://gpu again all graphics features have changed to "Software only". The chromium log the message is "GpuProcessHostUIShim: The GPU process crashed!".

Has anyone any idea why this is happening. I saw this first on our own board based on the SabreSD so then tried it on a actual SabreSD board with the same result.

Thanks in advance

Ian

ラベル(4)
0 件の賞賛
返信
1 返信

2,915件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ian,

I guess you need to go to chrome://flags and enable "Override software rendering list" and use the button on the bottom of that page to restart Chrome. Then when you have Chrome opened again go to chrome://gpu and everything should be hardware accelerated.

Hope this helps

0 件の賞賛
返信