Problems with GPU process crashing in Chromium

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems with GPU process crashing in Chromium

2,535 次查看
IanCraig
Contributor II

Hi

I'm trying to get Chromium running on the SabreSD board and having problems with the GPU process crashing when opening a web page. My setup is as follows

FSL Community BSP 1.8 Fido

Kernel 3.14.28-1.0.0_ga+g91cf351

core-image-sato image with chromium (40.0.2214.91) added

Freescale SabreSD board

On boot chromium reports hardware acceleration is enabled and everything looks fine but as soon as you open a web page and check chrome://gpu again all graphics features have changed to "Software only". The chromium log the message is "GpuProcessHostUIShim: The GPU process crashed!".

Has anyone any idea why this is happening. I saw this first on our own board based on the SabreSD so then tried it on a actual SabreSD board with the same result.

Thanks in advance

Ian

标签 (4)
0 项奖励
回复
1 回复

1,683 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ian,

I guess you need to go to chrome://flags and enable "Override software rendering list" and use the button on the bottom of that page to restart Chrome. Then when you have Chrome opened again go to chrome://gpu and everything should be hardware accelerated.

Hope this helps

0 项奖励
回复