Problems with CS1 control fail when using EIM interface in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with CS1 control fail when using EIM interface in u-boot

3,632 Views
haesungjung
Contributor I

Dear community,

We occured the following problems during testing on the reference SABRESD board(MCIMX6Q-SDB).
Problems with CS1 control fail when using EIM interface in u-boot

** Questions  **
- Is the below setting correct?
- In kernel, success to write data to EIM CS0 / CS1 using ioremap function.
  In uboot environment, how to write data to an address without ioremap function?

The environment and settings are shown below.
1. uboot version : v2013.10-r0

2. Kernel version : L3.0.35-r37.14

3. modify u-boot source code

- file : board/freescale/mx6sabresd

- function : board_late_init()

- PAD Setting

iomux_v3_cfg_t   weim_pads[] = {
    MX6_PAD_EIM_OE__WEIM_WEIM_OE | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_RW__WEIM_WEIM_RW | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_CS0__WEIM_WEIM_CS_0 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_CS1__WEIM_WEIM_CS_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),

    MX6_PAD_EIM_LBA__WEIM_WEIM_LBA | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_BCLK__WEIM_WEIM_BCLK | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_EB1__WEIM_WEIM_EB_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),

    MX6_PAD_EIM_DA15__WEIM_WEIM_DA_A_15 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA14__WEIM_WEIM_DA_A_14 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA13__WEIM_WEIM_DA_A_13 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA12__WEIM_WEIM_DA_A_12 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA11__WEIM_WEIM_DA_A_11 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA10__WEIM_WEIM_DA_A_10 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA9__WEIM_WEIM_DA_A_9 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA8__WEIM_WEIM_DA_A_8 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA7__WEIM_WEIM_DA_A_7 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA6__WEIM_WEIM_DA_A_6 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA5__WEIM_WEIM_DA_A_5 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA4__WEIM_WEIM_DA_A_4 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA3__WEIM_WEIM_DA_A_3 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA2__WEIM_WEIM_DA_A_2 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA1__WEIM_WEIM_DA_A_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_DA0__WEIM_WEIM_DA_A_0 | MUX_PAD_CTRL(EIM_PAD_CTRL),

    MX6_PAD_CSI0_DAT12__WEIM_WEIM_D_8 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT13__WEIM_WEIM_D_9 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT14__WEIM_WEIM_D_10 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT15__WEIM_WEIM_D_11 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT16__WEIM_WEIM_D_12 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT17__WEIM_WEIM_D_13 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT18__WEIM_WEIM_D_14 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_CSI0_DAT19__WEIM_WEIM_D_15 | MUX_PAD_CTRL(EIM_PAD_CTRL),

    MX6_PAD_EIM_A16__WEIM_WEIM_A_16 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A17__WEIM_WEIM_A_17 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A18__WEIM_WEIM_A_18 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A19__WEIM_WEIM_A_19 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A20__WEIM_WEIM_A_20 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A21__WEIM_WEIM_A_21 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A22__WEIM_WEIM_A_22 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A23__WEIM_WEIM_A_23 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A24__WEIM_WEIM_A_24 | MUX_PAD_CTRL(EIM_PAD_CTRL),
    MX6_PAD_EIM_A25__WEIM_WEIM_A_25 | MUX_PAD_CTRL(EIM_PAD_CTRL)
};

              imx_iomux_v3_setup_multiple_pads(weim_pads,ARRAY_SIZE(weim_pads));

- IOMUXC_GPR1 / CS1GCR1 / CS1GCR2 / CS1RCR1 / CS1RCR2 / CS1WCR1 / CS1WCR2 / CS1WCR Setting

                    EIM_configuration.JPG

   void  __iomem *eim_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR +0x18);

//GPR1 register/////////////////////////////////////////////////////////////////////
   reg = readl(IOMUXC_BASE_ADDR + 0x4);   // GPR1 register  CS0/CS1 enable
   reg &= ~0x07ffffff;
   reg |= 0x1b;
   writel(reg, IOMUXC_BASE_ADDR + 0x4);

//CS1GCR1///////////////////////////////////////////////////////////////////////////
   writel(0x00051081,eim_reg);    //CS1GC[18:16](DSZ -> 101 : 8bit port resides on DATA[15:8]
//CS1GCR2///////////////////////////////////////////////////////////////////////////
   writel(0x00000000,(eim_reg+ 0x4));    //CS1GCR2
//CS1RCR1///////////////////////////////////////////////////////////////////////////
   writel(0x16000202,(eim_reg+ 0x8));    //CS1RCR1
//CS1RCR2///////////////////////////////////////////////////////////////////////////
   writel(0x00000002,(eim_reg+ 0xC));    //CS1RCR2
//CS1WCR1///////////////////////////////////////////////////////////////////////////
   writel(0x16002082,(eim_reg+ 0x10));    //CS1WCR1
//CS1WCR2///////////////////////////////////////////////////////////////////////////
   writel(0x00000000,(eim_reg+ 0x14));    //CS1WCR2
//CS1WCR////////////////////////////////////////////////////////////////////////////
   writel(0x00000000,(eim_reg+ 0x90));    //CS1WCR

- Data Write
        *(unsigned char *)(0x8400000) = 0x0A; // CS0
        *(unsigned char *)(0xC400000) = 0x0A; // CS1

4. How to check the operation
- Check EIM CS1(R627) operation using oscilloscope

R627.jpg

5. Test result
- EIM CS1 pin does not move

Wave.jpg
- When writing data (*(unsigned char *)(0x8400000) = 0x0A;) ,
  uboot init no longer proceeds and kernel is not loaded.
 

0 Kudos
Reply
5 Replies

3,360 Views
haesungjung
Contributor I

Dear igor,

Thank you for quickly response.

In the kernel, both CS0 and CS1 are successfully written.
So in uboot, We set the same value as in Kernel for the following registers.
IOMUXC_GPR1 / CS1GCR1 / CS1GCR2 / CS1RCR1 / CS1RCR2 / CS1WCR1 / CS1WCR2 / CS1WCR

We want to access EIM CS1 using the ioremap function as in the kernel.
We understand that to use the ioremap function, we must enable the MMU.Is right?

Please let us know, How can We enable the MMU in uboot?

0 Kudos
Reply

3,360 Views
igorpadykov
NXP Employee
NXP Employee

please look at

How to enable yocto uboot MMU? 

Best regards
igor

0 Kudos
Reply

3,360 Views
haesungjung
Contributor I

Dear Igor,

Thank you for your answer.
We have worked again with the eim paralle nor example in mx6qsabreauto.c file.

We use CS0 (64MB), CS1 (64MB) and write data to CS0 and CS1 respectively as shown below.

CS0 write succeeds, but a fault occurs when writing to CS1.

* (unsigned char *) (0x8400000) = 0x0A; // CS0 Write -> Success
udelay (100);
* (unsigned char *) (0xC400000) = 0x0A; // CS1 Write -> Fail

In Kernel, write is successful in both CS0 and CS1 using ioremap function.


Is there anything else I need to do to write using CS1 in uboot?

If enable MMU in uboot, can ioremap be used?
if so, Is there a way to enable the MMU in uboot?

Thank you for your help.

0 Kudos
Reply

3,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi HAE

in uboot one can printf eim cs0, cs1 settings and compare them.

Also one can check iomux cs1 settings.

Best regards
igor

0 Kudos
Reply

3,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi HAE

parallel nor is used with eim on sabre ai board and one can look at its uboot:

uboot/board/freescale/mx6qsabreauto/mx6qsabreauto.c

uboot-imx.git - Freescale i.MX u-boot Tree 

In particular one can check if eim clock is enabled in CCM_CCGR6

As SABRESD board (MCIMX6Q-SDB) uses EIM signals for other
purposes, one needs to check uboot code and remove EIM signals from
usage by other modules.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply