Problems modifying device tree to blink an LED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems modifying device tree to blink an LED

ソリューションへジャンプ
21,047件の閲覧回数
rathben
Contributor III

Hello All -

I've had a surprising amount of difficulty trying to figure out how to use dts to configure the hardware to heartbeat-blink the debug led on the i.MX6SL EVK. I'm running kernel 3.10.17, building core-image-minimal, and tried adding the following code in the appropriate places in imx6sl-evk.dts (as well as enabling the appropriate items in the kernel menuconfig):

  leds {

  compatible = "gpio-leds";

  debug-led {

  label = "Heartbeat";

  gpios = <&gpio3 20 0>; //HSIC_STROBE -> GPIO3_20

  linux,default-trigger = "heartbeat";

  };

  };

and

  MX6SL_PAD_HSIC_STROBE__GPIO3_IO20 0x110b0

After much trial and error, I was able to get this to work after modifying the init function register_init_complete (in .../git/drivers/regulator/core.c) to return early without doing anything.

I'm looking into this further, but in the meantime, does anyone have any ideas about what is going on here?

Thanks! -Ben

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
15,197件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ben,

Please try this patch that I have just submitted:

'[PATCH] ARM: dts: imx6sl-evk: Keep VGEN1 regulator always enabled' - MARC

Regards,

Fabio Estevam

元の投稿で解決策を見る

0 件の賞賛
返信
20 返答(返信)
15,197件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ben,

I have just tested with this changes and it works here:

--- a/arch/arm/boot/dts/imx6sl-evk.dts

+++ b/arch/arm/boot/dts/imx6sl-evk.dts

@@ -19,6 +19,18 @@

                reg = <0x80000000 0x40000000>;

        };

+       leds {

+               compatible = "gpio-leds";

+               pinctrl-names = "default";

+               pinctrl-0 = <&pinctrl_led>;

+

+               user {

+                       label = "Heartbeat";

+                       gpios = <&gpio3 20 0>;

+                       linux,default-trigger = "heartbeat";

+               };

+       };

+

        regulators {

                compatible = "simple-bus";

                #address-cells = <1>;

@@ -108,6 +120,12 @@

                        >;

                };

+               pinctrl_led: ledgrp {

+                       fsl,pins = <

+                               MX6SL_PAD_HSIC_STROBE__GPIO3_IO20 0x17059

+                       >;

+               };

+

                pinctrl_kpp: kppgrp {

                        fsl,pins = <

                                MX6SL_PAD_KEY_ROW0__KEY_ROW0    0x1b010

Regards,

Fabio Estevam

15,197件の閲覧回数
rathben
Contributor III

same result as with Marek's suggestions. Side note, is there a significance to you placing the pinctrl_led node in regulators while Marek suggested iomuxc? Also I noticed that your patch is not based from the same version of imx6sl-evk.dts as mine. Is there something else in the file that I might be missing?

0 件の賞賛
返信
15,197件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I haven't put the pinctrl_led node into regulators. The patch I sent is against 3.14-rc1. Haven't tested 3.10 yet.

Regards,

Fabio Estevam

0 件の賞賛
返信
15,197件の閲覧回数
rathben
Contributor III

ok. I've placed pinctrl_led in the &iomuxc node as follows, is this correct? (still doesn't work, but at least we'll be on the same page)

&iomuxc {

  pinctrl-names = "default", "sleep";

  pinctrl-0 = <&pinctrl_hog>;

  pinctrl-1 = <&pinctrl_hog_sleep>;

   pinctrl_led: ledgrp {

           fsl,pins = <

                   MX6SL_PAD_HSIC_STROBE__GPIO3_IO20 0x17059

           >;

   };

  hog {

  pinctrl_hog: hoggrp {

  fsl,pins = <

  MX6SL_PAD_KEY_ROW7__GPIO4_IO07    0x17059

0 件の賞賛
返信
15,196件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Here is a patch against 3.10.17.

I won't have access to my mx6slevk until tomorrow to test it.

0 件の賞賛
返信
15,195件の閲覧回数
rathben
Contributor III

thanks for the patch, but same non-working result

0 件の賞賛
返信
15,195件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ben,

Today I tested 3.14-rc1 and got the LEDs blinking on my mx6slevk at the office.

Running the same 3.14-rc1 kernel and dtb on the mx6slevk I have at home I got no LED blinking.

I don't have a scope here at home to measure the signals. The evk I have at home is an old version (it is a red one).

Tomorrow I will try 3.10 with the evk from the office.

Regards,

Fabio Estevam

0 件の賞賛
返信
15,195件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ok, so I tested on 3.10 and I see the same behavior as you reported: LED blinks once and then stops.

If I run 3.14-rc1 it works fine though.

Also tested 3.10.17 on a mx53qsb and the LED blinks fine.

I haven't had a chance to debug this.

Regards,

Fabio Estevam

0 件の賞賛
返信
15,195件の閲覧回数
rathben
Contributor III

well... I guess that is "good" news, at least we're seeing the same behavior and I'm apparently not totally insane :smileyhappy:. You might try commenting out the call to regulator_init_complete (same as I did) to see that it works afterwards. Perhaps someone shedding some light on what this function does might help to debug the situation. Thanks!

0 件の賞賛
返信
15,198件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ben,

Please try this patch that I have just submitted:

'[PATCH] ARM: dts: imx6sl-evk: Keep VGEN1 regulator always enabled' - MARC

Regards,

Fabio Estevam

0 件の賞賛
返信
15,190件の閲覧回数
rathben
Contributor III

This works for me. Thanks!

0 件の賞賛
返信
15,195件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Some more hints:

Stop the heartbeat blinking:

$ echo none >  /sys/class/leds/Heartbeat/trigger

Turn on the LED:

$ echo 1 > /sys/class/leds/Heartbeat/brightness

Turn off the LED:

$ echo 0 > /sys/class/leds/Heartbeat/brightness

Regards,

Fabio Estevam

0 件の賞賛
返信
15,195件の閲覧回数
MarekVasut
Senior Contributor I

Check if you have the necessary stuff enabled in your kernel config ...

$ grep LED_TRIGGERS .config

$ grep LEDS_TRIGGER_HEARTBEAT .config

$ grep LEDS_GPIO .config

Next, check if your pin is really configured as GPIO. I don't see

                pinctrl-names = "default";

                pinctrl-0 = <&led_pin_gpio>;

anywhere in your led {} DT node. You should have those two right under the 'compatible' prop AND the led_pin_gpio should be defined in the &iomuxc node like so:

                led_pin_gpio: led_gpio@0 {

                        fsl,pins = <

                                MX6SL_PAD_HSIC_STROBE__GPIO3_IO20            0x110b0

                        >;

                };

You can use /sys/class/leds/*/brightness to toggle the led when debugging this stuff.

15,195件の閲覧回数
rathben
Contributor III

this is helpful but doesn't work for me. I can see that during bootup the led blinks once and then stops around the time that regulator_init_complete runs

0 件の賞賛
返信
15,195件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

It should be

MX6SL_PAD_HSIC_STROBE__GPIO3_IO20 0x80000000

Regards,

Fabio Estevam

0 件の賞賛
返信
15,195件の閲覧回数
rathben
Contributor III

Hi Fabio, thanks for your response. Please clarify. What is the significance of this value? The 31st bit isn't defined by any documentation I've seen. I will double-check tomorrow but I believe I did try this value before going on my frantic adventure commenting out initialization functions out until it worked.

0 件の賞賛
返信
15,195件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

It is documented at:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/p...

"Bits used for CONFIG:
NO_PAD_CTL(1 << 31): indicate this pin does not need config."

So the LED still does not work?

Regards,

Fabio Estevam

0 件の賞賛
返信
15,195件の閲覧回数
rathben
Contributor III

changing the pad config to 0x80000000 did not get the led to work. I will go on to trying the other suggestions below

0 件の賞賛
返信
15,195件の閲覧回数
MarekVasut
Senior Contributor I

That NO_PAD_CTL means 'don't touch the current configuration of the pin, it was configured by bootloader', right ?

0 件の賞賛
返信
15,196件の閲覧回数
rathben
Contributor III

thank you for the documentation link, I'll try it tomorrow when I get back to the hardware. Thanks!

0 件の賞賛
返信