Problems building ltib (elftosb missing)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems building ltib (elftosb missing)

跳至解决方案
2,526 次查看
dafmulder
Contributor I

Hello there,

I've a serious problem building my ltib. (for an analogue of the imx53 qsb)

The problem is the elftosb-11.09.01.tar.gz.md5 package which is not available online anymore.

I already tried working my way around it by using the source package for imx6 which has a 10.0.01 version of elftosb but to no avail.

Maybe there is someone with this package still somewhere or a different approach to it.

Error:

Try elftosb-11.09.01.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz.md5:

16:42:21 ERROR 404: Not Found.

Try elftosb-11.09.01.tar.gz from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz:

16:42:22 ERROR 404: Not Found.

Can't get: elftosb-11.09.01.tar.gz at ./ltib line 790.

Died at ./ltib line 1380.

traceback:

main::build_host_rpms:1380

  main::host_checks:1435

   main:542


标签 (1)
标记 (5)
0 项奖励
回复
1 解答
1,626 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
1,629 次查看
dafmulder
Contributor I

Thank you, I eventually got it working with the 12.04LTIB

0 项奖励
回复
1,627 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复