Problems building ltib (elftosb missing)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems building ltib (elftosb missing)

ソリューションへジャンプ
2,416件の閲覧回数
dafmulder
Contributor I

Hello there,

I've a serious problem building my ltib. (for an analogue of the imx53 qsb)

The problem is the elftosb-11.09.01.tar.gz.md5 package which is not available online anymore.

I already tried working my way around it by using the source package for imx6 which has a 10.0.01 version of elftosb but to no avail.

Maybe there is someone with this package still somewhere or a different approach to it.

Error:

Try elftosb-11.09.01.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz.md5:

16:42:21 ERROR 404: Not Found.

Try elftosb-11.09.01.tar.gz from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz:

16:42:22 ERROR 404: Not Found.

Can't get: elftosb-11.09.01.tar.gz at ./ltib line 790.

Died at ./ltib line 1380.

traceback:

main::build_host_rpms:1380

  main::host_checks:1435

   main:542


ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
1,516件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
1,519件の閲覧回数
dafmulder
Contributor I

Thank you, I eventually got it working with the 12.04LTIB

0 件の賞賛
返信
1,517件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信