Problems adding olsrd package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems adding olsrd package

2,243件の閲覧回数
unaigonzalez
Contributor II

I have this error trying to add olsrd package:

plc@ubuntu:~/ltib$ sudo ./ltib -m prep -p olsrd.spec

[sudo] password for plc:

You should not be root when running ltib, do you really

want to continue ? y|N

y

Processing: olsrd

===================

/home/plc/ltib/dist/lfs-5.1/olsrd-0.5.6-r8.tar.gz/olsrd.spec does

not contain an entry for Name: at /home/plc/ltib/bin/Ltibutils.pm

line 188.

Died at ./ltib line 752.

traceback:

main::build_rpm:752

main::f_prep:992

main:560

Exiting on error or interrupt

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

2,022件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Unai,

I've never try to add Olsrd package, but packages need to be added from the host libraries to the ltibutil.pm, please check

Best image for iMX6 Sabre Lite Board ?

Also, instead of ltib you should try to move to Yocto BSP.

Hope this helps

Have a great day,
Alfredo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,022件の閲覧回数
unaigonzalez
Contributor II

Hay Bio,

I was trying to add manually the packages, i follow this steps:

1. copy source in /opt/freescale/pkgs
2. create file source_name.md5
md5sum source_name > source_name.md5
3. create directory in <you_ltib_dir>dist/lfs-5.1/<you_package> and copy spec-file to it

After this you can use ltib for build package:
1. ./ltib -m prep -p package.spec
2. ./ltib -m scbuild -p package.spec
3. ./ltib -m scdeploy -p package.spec

But the posted erro appear and I am pretty lost

0 件の賞賛
返信