Problem with the change frequency of the horizontal sync HorizSync Android IMX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with the change frequency of the horizontal sync HorizSync Android IMX

1,129 Views
andreylipov
Contributor II

Hello,

I have Imx6Q with android 4.2

I am trying to connect a non-standard display with a resolution of 640 by 240.

Connect it by LCD TTL.

Horizontal Sync of my monitor is 15.38 kilohertz.

All modes are registered in modedb.c start from 31.5 kHz.

I know that Linux have /etc/X11/xorg.conf where you can set the range from where to where.

Where to change the Horizontal Sync on Android?

I tried to create a new driver in the video / mxc / and write it in mxc_lcdif.c, after starting the FB the resolution changes but the Horizontal Sync remains the same or even displays nonsense

I would be grateful for any help and tips.

Andrey.

0 Kudos
Reply
0 Replies